MC9S08GT60 SCI baud rate modulo divisor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S08GT60 SCI baud rate modulo divisor

3,580 Views
cschai
Contributor I
hi,
anyone has MC8S08GT60 SCI baud rate modulo divisor table, register SCIxBDH and SCIxBDL (SBR12:smileyfrustrated:BR0)?
i cant find in the data sheet. Freescale should have included it.

Thanks.
Labels (1)
0 Kudos
Reply
4 Replies

1,099 Views
peg
Senior Contributor IV
Hi cschai,
 
It is easiest to use the spreadsheet in AN2494 for this, helps with all clock related issues as well.
 
Also you may be able to dig out some old posts by me on achieving "standard" baudrates on these devices.
 
0 Kudos
Reply

1,099 Views
cschai
Contributor I
thanks!
but did AN2494 really tell the SCI baud rate divisor? it just explain the ICG, is it?
i cant find any SCI baud rate divisor table in AN2494 although it did mention about SCI baud rate!

for example:
if my bus freq = 8Mhz
required baud rate = 19200
from baud rate = bus freq / (16*SBR)
thus SBR ~= 26

what is the setting of SBR to get approximate baud rate divisor of 26?

thanks!
0 Kudos
Reply

1,099 Views
peg
Senior Contributor IV
Hi,
 
There is no actual table as it is just the raw 13-bit binary value (e.g. 1=1, 2=2 and 3=3 etc). Mostly you just clear the high register and load the divisor into the low one (as it generally fits in one byte).
The associated spreadsheet with the quoted AN will tell you exactly what to load if you plug in all your details.
 
In your case the 26dec just goes straight into the low byte of the register (with high byte cleared)
 

Message Edited by peg on 2007-02-0901:23 PM

0 Kudos
Reply

1,099 Views
cschai
Contributor I
Peg,

Thanks....
0 Kudos
Reply