Hi,
I suppose that you want to use RTI in run (normal operating) mode...in the mode RTI don't run with internal oscillator - Manual for GT60 p. 67 ... or a PE bean warning :
+TI1
+Warning: RTI device won't run in Run mode - Internal oscillator is selected as clock source!
Regards, Processor Expert Support
 
					
				
		
Message Edited by alex_spotw on 02-23-200601:48 PM
 
					
				
		
Hi all,
Woops it's pretty darn clear...
"In run and wait modes, only the external clock can be used as the RTI's clock source. In stop2 mode, only the internal RTI clock can be used."
I would like to know the reason behind why the RTI does not have access to this clock in run mode.
Some reasons why you would want this.
With a high frequency xtal the divider is not enough!
With no xtal (SCM, FEI) you have got no RTI at all (in run mode).
As to the warning (or lack of) from Processor Expert:
You may be using the RTI purely as a method of exit from STOP mode so the setup would be valid. As is often the case the answer is to RTFM!
Peg
 
					
				
		
Hi Alex,
If you have got it working with the external osc, then it should just be a matter of changing SRTISC from 0x37 to 0x17. The RTI period will change from 2ms to 1s though. Why don't you try to do a clock select change "on the fly" in your code? If it stops giving interrupts then your internal RTI clock is broke.
BTW there is an error in the GB60 manual Rev2.3 at 5.8.6 (SRTISC) it says there is 3 unimplemented bits, there is only 1!
BR
Peg
 
					
				
		
 
					
				
		
Hi Alex,
Not what you want to hear, but I confirm your observation using the code below on a GB60 with 3L31R. 
BTW 32kHz xtal.
NOLIST
#include "9S08GB60v1rdp.inc"
.LIST
 ORG RamStart
counter  rmb 1
stat rmb 1
ORG RomStart
 lda #(mCOPT+mSTOPE+mBKGDPE)
 sta SOPT   ;disable COP
 mov #0,counter
 mov #%00001111,PTFD
 mov #%00001111,PTFDD
 mov #mPTAPE4,PTAPE
 clr stat
 ldhx #$0000
*********** Set-up ICG to clock the bus at 18.8 MHz **********************
  MOV #(mMFD2|mMFD1|mMFD0),ICGC2 ;sets MFD divider
  MOV #(mREFS|mCLKS1|mCLKS0),ICGC1  ;
  BRCLR LOCK,ICGS1,*  ;loop until FLL locks
 jsr RTI_init
 CLI    ;enable ints
loop1 brset PTAD4,PTAD,loop2
 brset 0,stat,loop1
 bset 0,stat
 lda SRTISC
 ora #mRTICLKS
 sta srtisc
 bra loop1
loop2 brclr 0,stat,loop1
 bclr 0,stat
 lda SRTISC
 eor #mRTICLKS
 sta srtisc
 bra loop1
RTI_init:
* lda #(mRTICLKS+mRTIE+mRTIS2+mRTIS1+mRTIS0)
 lda #(mRTIE+mRTIS2+mRTIS1+mRTIS0)
 sta SRTISC
 rts
RTI_Handler:
 lda SRTISC
 ora #mRTIACK
 sta srtisc
 inc counter
 lda counter
 coma
 sta PTFD
 rti
 ORG $FFCC
 DC.W RTI_Handler ; RTI
 ORG $FFFE
 DC.W ROMStart ;
BR
Peg