Hi,
I suppose that you want to use RTI in run (normal operating) mode...in the mode RTI don't run with internal oscillator - Manual for GT60 p. 67 ... or a PE bean warning :
+TI1
+Warning: RTI device won't run in Run mode - Internal oscillator is selected as clock source!
Regards, Processor Expert Support
Message Edited by alex_spotw on 02-23-200601:48 PM
Hi all,
Woops it's pretty darn clear...
"In run and wait modes, only the external clock can be used as the RTI's clock source. In stop2 mode, only the internal RTI clock can be used."
I would like to know the reason behind why the RTI does not have access to this clock in run mode.
Some reasons why you would want this.
With a high frequency xtal the divider is not enough!
With no xtal (SCM, FEI) you have got no RTI at all (in run mode).
As to the warning (or lack of) from Processor Expert:
You may be using the RTI purely as a method of exit from STOP mode so the setup would be valid. As is often the case the answer is to RTFM!
Peg
Hi Alex,
If you have got it working with the external osc, then it should just be a matter of changing SRTISC from 0x37 to 0x17. The RTI period will change from 2ms to 1s though. Why don't you try to do a clock select change "on the fly" in your code? If it stops giving interrupts then your internal RTI clock is broke.
BTW there is an error in the GB60 manual Rev2.3 at 5.8.6 (SRTISC) it says there is 3 unimplemented bits, there is only 1!
BR
Peg
Hi Alex,
Not what you want to hear, but I confirm your observation using the code below on a GB60 with 3L31R. ![]()
BTW 32kHz xtal.
NOLIST
#include "9S08GB60v1rdp.inc"
.LIST
ORG RamStart
counter rmb 1
stat rmb 1
ORG RomStart
lda #(mCOPT+mSTOPE+mBKGDPE)
sta SOPT ;disable COP
mov #0,counter
mov #%00001111,PTFD
mov #%00001111,PTFDD
mov #mPTAPE4,PTAPE
clr stat
ldhx #$0000
*********** Set-up ICG to clock the bus at 18.8 MHz **********************
MOV #(mMFD2|mMFD1|mMFD0),ICGC2 ;sets MFD divider
MOV #(mREFS|mCLKS1|mCLKS0),ICGC1 ;
BRCLR LOCK,ICGS1,* ;loop until FLL locks
jsr RTI_init
CLI ;enable ints
loop1 brset PTAD4,PTAD,loop2
brset 0,stat,loop1
bset 0,stat
lda SRTISC
ora #mRTICLKS
sta srtisc
bra loop1
loop2 brclr 0,stat,loop1
bclr 0,stat
lda SRTISC
eor #mRTICLKS
sta srtisc
bra loop1
RTI_init:
* lda #(mRTICLKS+mRTIE+mRTIS2+mRTIS1+mRTIS0)
lda #(mRTIE+mRTIS2+mRTIS1+mRTIS0)
sta SRTISC
rts
RTI_Handler:
lda SRTISC
ora #mRTIACK
sta srtisc
inc counter
lda counter
coma
sta PTFD
rti
ORG $FFCC
DC.W RTI_Handler ; RTI
ORG $FFFE
DC.W ROMStart ;
BR
Peg