MC9S08GB32CFU: Identify mask revision with code?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S08GB32CFU: Identify mask revision with code?

2,482件の閲覧回数
BlkStang
Contributor I
Although I'm specifically working with a GB32CFU, this question could apply to other variants of the 9S08 family:

Is it possible to read the silicon mask revision (e.g. 3L31R) my code is running on?

We have increasingly stringent configuration controls being implemented and am being asked if we can automatically detect and react to an unexpected mask revision...


ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,445件の閲覧回数
JimDon
Senior Contributor III
System Device Identification Register (SDIDH, SDIDL) claims to have a revision number,

"The high-order 4 bits of address SDIDH are hard coded to reflect the current mask set
revision number"

But it seems on some parts the spec seems to imply they are always 0.





Message Edited by JimDon on 2008-03-13 05:25 PM
0 件の賞賛
返信

1,445件の閲覧回数
BlkStang
Contributor I
Looks like I can get a revision number from 0-F. This will probably work for me.

Thanks very much.

0 件の賞賛
返信