MC9S08DZ60CLC Sector Erase Time

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC9S08DZ60CLC Sector Erase Time

2,143 次查看
rsheldon
Contributor II

My application requires a fast sector erase/write time to function as a counter.  The measured erase/write time on my MC9S08DZ60CLC has been consistently about 3ms, however, the datasheet (p. 53) states that a sector erase by itself takes 20ms.  How is this possible?  Did I miss something or does the microcontroller perform better than it's supposed to? 

标签 (1)
0 项奖励
回复
5 回复数

1,304 次查看
kef
Specialist I

Looks like something is wrong with FCDIV setting. Timing is shorter almost 8 times, as if PRDIV8 bit was not set... Did you note that according to DZ60 datasheet FCDIV is write once register? This means you can't set up DIV5:0 bits first, and then set up PRDIV8 bit. All FCDIV bits should be written at once.

 

0 项奖励
回复

1,304 次查看
rsheldon
Contributor II

I should explain also that I am just learning assembly language and am trying to understand how a former employee coded our chip.  With that said, I took a look at the code and I found one line containing FCDIV that reads as follows:

 

 ; FCDIV: DIVLD=0,PRDIV8=0,DIV5=1,DIV4=0,DIV3=1,DIV2=0,DIV1=0,DIV0=1
            LDA     #$05 ;#$45       ;#$05 is for low
            STA     FCDIV                  ; Set clock divider

 

I hope this is useful information, if not let me know and I can scrounge up some more code.

 

0 项奖励
回复

1,304 次查看
bigmac
Specialist III

Hello,

 

The required FCDIV setting will depend on the bus frequency you are using - the divider setting must be such that a flash clock frequency within the range 150-200 kHz is generated. A divider setting of 5 will produce a division ratio of 6, implying that the bus clock is within the range 0.9-1.2 MHz.  However, I would suspect that this is probably not the case.

 

For example, if the bus frequency were 8 MHz, a divider setting of decimal 39 would be necessary.

 

Regards,

Mac

 

0 项奖励
回复

1,304 次查看
rsheldon
Contributor II

This appears to be the section of code in question:

 

;;; Drop down to 4MHz

        ; MCGC2: BDIV=0,RANGE=0,HGO=0,LP=0,EREFS=0,ERCLKEN=0,EREFSTEN=0
        ;CLR     MCGC2                  ; Set MCGC2 register
            MOV     #$40,MCGC2
        ; MCGC1: CLKS=0,RDIV=4,IREFS=1,IRCLKEN=1,IREFSTEN=0
            MOV     #$1E,MCGC1       ;#$26 for low #$06 for high
        ; MCGC3: LOLIE=0,PLLS=0,CME=0,VDIV=1
            MOV     #$01,MCGC3             ; Set MCGC3 register

        ; ### Init_FLASH init code
        ; FSTAT: FCBEF=0,FCCF=0,FPVIOL=1,FACCERR=1,FBLANK=0
            LDA     #%00110000
            STA     FSTAT                  ; Clear error flags
        ; FCDIV: DIVLD=0,PRDIV8=0,DIV5=1,DIV4=0,DIV3=1,DIV2=0,DIV1=0,DIV0=1
            LDA     #$05 ;#$45       ;#$05 is for low
            STA     FCDIV                  ; Set clock divider

 

It looks as if he loaded the accumulator with 0x05 and stored that value in FCDIV, but the comment shows he's setting FCDIV as 0x19. Am I interpreting this correctly?

0 项奖励
回复

1,304 次查看
bigmac
Specialist III

Hello,

 

It would appear that the code you have posted has been generated by the PE initialisation tool.  However, the FCDIV setting has then been altered without the comment line being updated.

 

  ; FCDIV: DIVLD=0,PRDIV8=0,DIV5=1,DIV4=0,DIV3=1,DIV2=0,DIV1=0,DIV0=1
           LDA     #$05 ;#$45       ;#$05 is for low
           STA     FCDIV            ; Set clock divider

 

 The original PE initialisation gives a value of $29 (decimal 41) for a division ratio of 42.  With this value, a trimmed bus frequency of nominally 8 MHz would give a flash clock frequency of 190 kHz, which makes allowance for a bus frequency tolerance of +/-5%. (This allowance would not be necessary if an external crystal reference were utilised.)

 

Accepting that the new bus frequency has been trimmed to 4 MHz, and allowing a similar frequency tolerance, the required division ratio would be 21.  Therefore the FCDIV setting should be $14 (20 decimal).

 

I suggest that you check the MCG register settings to determine whether the bus frequency is actually 4.0 MHz, as the initial comment suggests.

 

Regards,

Mac

 

0 项奖励
回复