Hi, I entercounted a problem about MC9S08DZ60 CAN. below is the specific description of the problem. Could any one help me on the issue?
I developed the below code to init the MCU and debug it in simulation mode on CW.
main()
{
.........
CAN_init(); // CAN initiate function
delay(); // delay 800ms
// transfer CAN to sleep mode
CANCTL0_SLPRQ =1;
while(!CANCTL1_SLPAK)
{
/*Refresh Watchdog*/
SRS = 0x55;
SRS = 0xAA;
}
CAN_init(); // recall CAN initiate function again.
..................
}
the detail code of function CAN_nit() listed below.
void CAN_init()
{
/*Perform CAN communication initializations*/
/*First enter the initialization state*/
CANCTL0 = ENTER_ININ_STATE;
/* loop to wait CAN enter initialization state */
while(!CANCTL1_INITAK)
{
/*Refresh Watchdog*/
SRS = 0x55;
SRS = 0xAA;
}
/*Select the clock source*/
CANCTL1 = CMCR1_INIT;
/*Set baud rate and prescaler*/
CANBTR1 = CBTR1_INIT;
CANBTR0 = CBTR0_INIT;
/*Set ID filter mode to Eight 8-bit Filters*/
CANIDAC = CIDAC_INIT;
/*initialize the CAN parameters*/
initCANParams();
/*initialize FIFO variables*/
ccrcvStatus = 0;
ccrcvBufGetPtr = ccrcvBufPutPtr = 0;
cctransBufGetPtr = cctransBufPutPtr = 0;
cctransbuffCount = ccrcvbuffCount = 0;
ccRcvErrors = ccTransErrors = 0;
ccnumRcv=0;
/*Return from Soft Reset State*/
CANCTL0 = EXIT__ININ_STATE;
/*Enable the error interrupts and the receive interrupt*/
CANRIER = CRIER_ERROR;
}
When I debug the code mentioned above, I found the code can be excuted normally before the second recall of function CAN_init(). I traced the code step by step and found when the function CAN_init was excuted in second time, the CAN can't enter into the initialization state because the flag INITAK in register CANCTL1 can't be set to 1. so the code drop into the loop and wait there forever.
my question is why the CAN INITAk flag can't be set to 1 at the second time while it can be set to 1 normally at first time. how to resolve this problem? Can I initiate the other CAN registers while INITAk flag is 0 and INITRQ is 1?