MC9S08DZ128CLH replacement part

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MC9S08DZ128CLH replacement part

跳至解决方案
2,057 次查看
nxf59945
NXP Employee
NXP Employee

Dear Sir:

Due to MC9S08DZ128CLH part shortage issue, my customer would like to survey if S9S08DZ128F2CLH could be replacement part without need to modify layout and firmware code, needs your comments to confirm, thanks!

B.R.

Eric

0 项奖励
回复
1 解答
2,043 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

 

your customer need to check if the errata for the mask set 2M78G (mask set for the auto part) are not affecting the part that normally used 

 

the pinout is the same and if the errata does not affect the customer program then, yes it is the same 

 

I hope this will help you

 

Regards

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,044 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

 

your customer need to check if the errata for the mask set 2M78G (mask set for the auto part) are not affecting the part that normally used 

 

the pinout is the same and if the errata does not affect the customer program then, yes it is the same 

 

I hope this will help you

 

Regards

 

0 项奖励
回复
2,039 次查看
nxf59945
NXP Employee
NXP Employee

Thanks Vicente's comments and instant help!

B.R.

Eric

0 项奖励
回复