MC9S08DN32

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S08DN32

1,760件の閲覧回数
lyong
Contributor I
Hello everybody, I have two problems on MC9S08DN32 would like to consult. 1. when the MC9S08DN32 using the internal reference clock, how much the highest multiplication frequency? 2. Internal reference clock with temperature (assuming no change in voltage). Best to have a temperature tolerance 。 Thanks!
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,301件の閲覧回数
bigmac
Specialist III

Hello, and welcome to the forum.

 

Assuming you are using FEI mode, the DCO frequency will be 1024 times the reference frequency.  This frequency is then divided by the BDIV factor, and a further divide by 2, to give the bus frequency.

 

After POR the default BDIV factor will be 2, so that the bus frequency would be 256 times the reference frequency, i.e. a bus frequency between the limits 8 MHz to10 MHz after the internal reference has been trimmed to the required frequency.

 

The frequency tolerance for the internal reference, over the temperature range 0C to 70C is given in the datasheet (Appendix A).

 

Regards,

Mac

 

0 件の賞賛
返信

1,301件の閲覧回数
lyong
Contributor I

Thank you very much!Ithink I am understand.

0 件の賞賛
返信