MC9S08 SRS / watchdog problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S08 SRS / watchdog problem

2,186件の閲覧回数
Nik
Contributor III

Hi,

 

I  have COP enabled.  If I put the program into a loop without a watchdog reset, the processor resets as expected.

But the SRS register alomost always is clear.  Sometimes the PIN bit is set, sometimes the COP bit is set, sometimes POR bit is set.  Most of the time the register is clear.  If I debug, and cause a watchdog timeout, the SRS_COP is set.

 

I just power up the project and I got a SRS_POR.  Then I reset the processor by the reset pin and got a SPS_POR.

 

Goofy as hell.  any ideas?

 

Thanks,

-

Robert

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,656件の閲覧回数
rocco
Senior Contributor II

Hi Robert,

 

What chip are you using?

 

On the GP32, the SRS register was reliable. But the same code running on the GB60 seems to experience what you are describing.

0 件の賞賛
返信

1,656件の閲覧回数
Nik
Contributor III

The part is the MC9S08JM60.  Do you know if there is there errata for this bug?  Is Freescale aware of this problem?  

 

Thanks,

Robert

0 件の賞賛
返信

1,656件の閲覧回数
rocco
Senior Contributor II

Hi Robert,

 

I have not found an errata, but I'm also not sure it is a bug in the chip.

 

My GB60 board is not yet in production, so the issue I'm seeing is through the debugger and the BDM. I have learned to take what I see in the debugger with a grain of salt. It could easily be a debugger problem.

 

I will know better once I'm running the GB60 standalone.

0 件の賞賛
返信