MC9S08 Programming Kit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MC9S08 Programming Kit

跳至解决方案
11,857 次查看
agustinc
Contributor II

Hello Everyone,

I have few finished boards with MC9S08 microcontrollers ready to be encased; however, there is a last minute update. The former programmer ask me to acquire a Freescale MCU Programming Kit in order to have the embedded code updated. There is a USB port ready for that purpose.

Since you have a bunch of kits, what Programming Kit do I need?

Thanks

标签 (1)
标记 (3)
1 解答
9,321 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

hi agustin.

you can use either BDM multilinik cable or Cyclone Pro for programming,.

here is BDM Multilink cable:

(http://www.pemicro.com/products/product_viewDetails.cfm?product_id=33&CFID=11365570&CFTOKEN=e12be3b7... )

Cyclone Pro is recommended for both development and production, while the Multilink cables are recommended only for development. This is the link for cyclone PRO. We can see it in below link:

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=1&menu_id=details&CFID=1605153&CF...

hope this helps!

===================================

this answer is for you, if it helps, please click on "correct answer" button. thanks!

Best Regards,

ZhangJun

在原帖中查看解决方案

0 项奖励
回复
6 回复数
9,322 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

hi agustin.

you can use either BDM multilinik cable or Cyclone Pro for programming,.

here is BDM Multilink cable:

(http://www.pemicro.com/products/product_viewDetails.cfm?product_id=33&CFID=11365570&CFTOKEN=e12be3b7... )

Cyclone Pro is recommended for both development and production, while the Multilink cables are recommended only for development. This is the link for cyclone PRO. We can see it in below link:

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=1&menu_id=details&CFID=1605153&CF...

hope this helps!

===================================

this answer is for you, if it helps, please click on "correct answer" button. thanks!

Best Regards,

ZhangJun

0 项奖励
回复
9,321 次查看
agustinc
Contributor II

Hello Jennie,

Thanks for your quick response. I see these tools connect to the board using the standard 6-pin connector (berg). However, there is no such pins on my boards, just a USB port. Is there any other way to program this MC9S08 MCU?

Thanks in advance.

0 项奖励
回复
9,321 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

hello agustin c,

do you use Freesale demo board? some of the demo board already integrated BDM emulator on board.

please let me know your board part number so that i can check it. thanks!

Best Regards,

Zhang Jun

9,321 次查看
agustinc
Contributor II

Hello Jennie,

We are actually looking into get a Universal Multilink Development Interface (http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=UMultilink&fsrch=1) to program our MC9S08 MCUs. Would that work?

Also, I realized the design doesn't include BDM pins but rather contacts to do the programming.

0 项奖励
回复
9,321 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

yes, UMultilink can support MC9S08 MCUs too, besides, UMultilink can also support HC(S)12(X), ColdFire V1/ColdFire+ V1, ColdFire V2-4, Qorivva MPC55xx/56xx, and Kinetis.


Best Regards,

Zhang Jun

9,321 次查看
agustinc
Contributor II

Hello Jennie,

I've been able to program my boards. Thanks for that.

However, I have another challenge now...I attached a dot-matrix lcd to my microcontroller and I've been trying to make it display anyhting...but still no luck.

Any chance you can help me out here? what is the sequence to have the lcd wonking?

Thanks a lot

agustin

0 项奖励
回复