MC9S08 Programming Kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S08 Programming Kit

Jump to solution
11,436 Views
agustinc
Contributor II

Hello Everyone,

I have few finished boards with MC9S08 microcontrollers ready to be encased; however, there is a last minute update. The former programmer ask me to acquire a Freescale MCU Programming Kit in order to have the embedded code updated. There is a USB port ready for that purpose.

Since you have a bunch of kits, what Programming Kit do I need?

Thanks

Labels (1)
Tags (3)
1 Solution
8,900 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi agustin.

you can use either BDM multilinik cable or Cyclone Pro for programming,.

here is BDM Multilink cable:

(http://www.pemicro.com/products/product_viewDetails.cfm?product_id=33&CFID=11365570&CFTOKEN=e12be3b7... )

Cyclone Pro is recommended for both development and production, while the Multilink cables are recommended only for development. This is the link for cyclone PRO. We can see it in below link:

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=1&menu_id=details&CFID=1605153&CF...

hope this helps!

===================================

this answer is for you, if it helps, please click on "correct answer" button. thanks!

Best Regards,

ZhangJun

View solution in original post

0 Kudos
Reply
6 Replies
8,901 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi agustin.

you can use either BDM multilinik cable or Cyclone Pro for programming,.

here is BDM Multilink cable:

(http://www.pemicro.com/products/product_viewDetails.cfm?product_id=33&CFID=11365570&CFTOKEN=e12be3b7... )

Cyclone Pro is recommended for both development and production, while the Multilink cables are recommended only for development. This is the link for cyclone PRO. We can see it in below link:

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=1&menu_id=details&CFID=1605153&CF...

hope this helps!

===================================

this answer is for you, if it helps, please click on "correct answer" button. thanks!

Best Regards,

ZhangJun

0 Kudos
Reply
8,900 Views
agustinc
Contributor II

Hello Jennie,

Thanks for your quick response. I see these tools connect to the board using the standard 6-pin connector (berg). However, there is no such pins on my boards, just a USB port. Is there any other way to program this MC9S08 MCU?

Thanks in advance.

0 Kudos
Reply
8,900 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hello agustin c,

do you use Freesale demo board? some of the demo board already integrated BDM emulator on board.

please let me know your board part number so that i can check it. thanks!

Best Regards,

Zhang Jun

8,900 Views
agustinc
Contributor II

Hello Jennie,

We are actually looking into get a Universal Multilink Development Interface (http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=UMultilink&fsrch=1) to program our MC9S08 MCUs. Would that work?

Also, I realized the design doesn't include BDM pins but rather contacts to do the programming.

0 Kudos
Reply
8,900 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

yes, UMultilink can support MC9S08 MCUs too, besides, UMultilink can also support HC(S)12(X), ColdFire V1/ColdFire+ V1, ColdFire V2-4, Qorivva MPC55xx/56xx, and Kinetis.


Best Regards,

Zhang Jun

8,900 Views
agustinc
Contributor II

Hello Jennie,

I've been able to program my boards. Thanks for that.

However, I have another challenge now...I attached a dot-matrix lcd to my microcontroller and I've been trying to make it display anyhting...but still no luck.

Any chance you can help me out here? what is the sequence to have the lcd wonking?

Thanks a lot

agustin

0 Kudos
Reply