MC9S08 3.3V operation.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S08 3.3V operation.

1,974 Views
sudheendra_varn
Contributor I

Hi,

 

    I want to clarify whether the following controllers can be operated on 3.3V

MC9S08SH8

MC9S08SE8.

    

The supply is very critical since we are looking at serial communication with another controller that is operating on 3.3V.

 

Also is there any other 8-bit controller with a pin count of 16 that can be operated at 3.3V.

 

Looking forward to your reply soon.

 

With regards,

S. Varna

Labels (1)
0 Kudos
Reply
2 Replies

1,415 Views
bigmac
Specialist III

Hello S. Varna, and welcome to the forum.

 

The '9S08SH8 and '9S08SE8 devices both have an allowable operating voltage range of 2.7 to 5.5 volts. They should be quite satisfactory if operating from a regulated 3.3 volt supply.

 

Regards,

Mac 

0 Kudos
Reply

1,415 Views
marbomb
Contributor I
I am using mc9s08qg8 which is 16 pin and runs on 3.3v.
0 Kudos
Reply