MC68HC908AZ32A programming

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MC68HC908AZ32A programming

跳至解决方案
1,770 次查看
vincentbergeron
Contributor I

Hi,

 

We have an usb multilink universal FX programmer and I was wondering if it was possible to program a MC68HC908AZ32A microcontroller with it.  We are using Code Warrior for Eclipse IDE 10.6.  If possible, can you please provide me with pin mapping and project setup please.

 

regards

标签 (1)
0 项奖励
回复
1 解答
1,661 次查看
john_suchyta
NXP Employee
NXP Employee

Hi Vincent,

The 908AZ32A is not supported by the Multilink Universal or CodeWarrior 10. This legacy device is supported by CodeWarrior 6.3 and the USB MON08 Multilink. CW 6.3 is a free download from our website. It only works on 32-bit PCs.

Regards,

John Suchyta

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,662 次查看
john_suchyta
NXP Employee
NXP Employee

Hi Vincent,

The 908AZ32A is not supported by the Multilink Universal or CodeWarrior 10. This legacy device is supported by CodeWarrior 6.3 and the USB MON08 Multilink. CW 6.3 is a free download from our website. It only works on 32-bit PCs.

Regards,

John Suchyta

0 项奖励
回复