MC68HC908AZ32A programming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC68HC908AZ32A programming

Jump to solution
1,709 Views
vincentbergeron
Contributor I

Hi,

 

We have an usb multilink universal FX programmer and I was wondering if it was possible to program a MC68HC908AZ32A microcontroller with it.  We are using Code Warrior for Eclipse IDE 10.6.  If possible, can you please provide me with pin mapping and project setup please.

 

regards

Labels (1)
0 Kudos
Reply
1 Solution
1,600 Views
john_suchyta
NXP Employee
NXP Employee

Hi Vincent,

The 908AZ32A is not supported by the Multilink Universal or CodeWarrior 10. This legacy device is supported by CodeWarrior 6.3 and the USB MON08 Multilink. CW 6.3 is a free download from our website. It only works on 32-bit PCs.

Regards,

John Suchyta

View solution in original post

0 Kudos
Reply
1 Reply
1,601 Views
john_suchyta
NXP Employee
NXP Employee

Hi Vincent,

The 908AZ32A is not supported by the Multilink Universal or CodeWarrior 10. This legacy device is supported by CodeWarrior 6.3 and the USB MON08 Multilink. CW 6.3 is a free download from our website. It only works on 32-bit PCs.

Regards,

John Suchyta

0 Kudos
Reply