MC68HC908AZ32A programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC68HC908AZ32A programming

ソリューションへジャンプ
1,750件の閲覧回数
vincentbergeron
Contributor I

Hi,

 

We have an usb multilink universal FX programmer and I was wondering if it was possible to program a MC68HC908AZ32A microcontroller with it.  We are using Code Warrior for Eclipse IDE 10.6.  If possible, can you please provide me with pin mapping and project setup please.

 

regards

ラベル(1)
0 件の賞賛
返信
1 解決策
1,641件の閲覧回数
john_suchyta
NXP Employee
NXP Employee

Hi Vincent,

The 908AZ32A is not supported by the Multilink Universal or CodeWarrior 10. This legacy device is supported by CodeWarrior 6.3 and the USB MON08 Multilink. CW 6.3 is a free download from our website. It only works on 32-bit PCs.

Regards,

John Suchyta

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,642件の閲覧回数
john_suchyta
NXP Employee
NXP Employee

Hi Vincent,

The 908AZ32A is not supported by the Multilink Universal or CodeWarrior 10. This legacy device is supported by CodeWarrior 6.3 and the USB MON08 Multilink. CW 6.3 is a free download from our website. It only works on 32-bit PCs.

Regards,

John Suchyta

0 件の賞賛
返信