MC68HC908AP32 with 60K flash?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC68HC908AP32 with 60K flash?

2,254 次查看
polosoft
Contributor I
Hi, first sorry for my english :smileysad:, I soldered a MC68HC908AP32 QFP44 by mistake instead of a HC908AP64. When I tried to save a 55K program ... it worked! :smileysurprised: . I double check flash an it was all there, no errors at all :smileyhappy: And the program running at 7.32MHz works ok.
 
So my question is how reliable can be flash above 32K in a HC908AP32? Or is this a Freescale mistake?
 
PD: I tested an old AP32 QFP44 purchased almost 2 years ago same mask and it also has 60K flash! Is this normal? :smileyindifferent:
 
Thanks a lot
 
标签 (1)
0 项奖励
回复
2 回复数

1,432 次查看
Alban
Senior Contributor II
Hello Polo,

This does happen and is not a mistake.
Creating a brand new masks costs a lot of money and some masks are used for several devices.

The extra memory and features that you may have will not have been tested.
So, it may work as it may not work.

Cheers,
Alban.
0 项奖励
回复

1,432 次查看
tonyp
Senior Contributor II
0 项奖励
回复