MC68HC908AP32 with 60K flash?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC68HC908AP32 with 60K flash?

2,232件の閲覧回数
polosoft
Contributor I
Hi, first sorry for my english :smileysad:, I soldered a MC68HC908AP32 QFP44 by mistake instead of a HC908AP64. When I tried to save a 55K program ... it worked! :smileysurprised: . I double check flash an it was all there, no errors at all :smileyhappy: And the program running at 7.32MHz works ok.
 
So my question is how reliable can be flash above 32K in a HC908AP32? Or is this a Freescale mistake?
 
PD: I tested an old AP32 QFP44 purchased almost 2 years ago same mask and it also has 60K flash! Is this normal? :smileyindifferent:
 
Thanks a lot
 
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,410件の閲覧回数
Alban
Senior Contributor II
Hello Polo,

This does happen and is not a mistake.
Creating a brand new masks costs a lot of money and some masks are used for several devices.

The extra memory and features that you may have will not have been tested.
So, it may work as it may not work.

Cheers,
Alban.
0 件の賞賛
返信

1,410件の閲覧回数
tonyp
Senior Contributor II
0 件の賞賛
返信