MC68HC705J5A programming specification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC68HC705J5A programming specification

4,029件の閲覧回数
Andik
Contributor II
Hello,
please, could someone help me to find a MC68HC705J5A programming specification? It's pretty old chip, but still in stock, and I have to develop a programmer for it. Freescale's support couldn't help.

Exact bootloader firmware contained in J5A or selfprogramming circuit design should help.
Thanks.
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,295件の閲覧回数
Alban
Senior Contributor II
Hello Andik,
 
I have schematics for a programmer of 705J1A from EPROM 2764, but are they compatible ?
 
Which mask are you refering to, please ?
 
Do you have the datasheet at least ?
 
Alban.
0 件の賞賛
返信

2,295件の閲覧回数
Andik
Contributor II

Alban wrote:

I have schematics for a programmer of 705J1A from EPROM 2764, but are they compatible ?

Which mask are you refering to, please ?

Do you have the datasheet at least ?

Alban.




Hi,
I have a doc named M68HC705JICSUM, which is a 705Jx simulator-programmer user manual, but this looks like not useful, because it's for J1, J2, and the sockets have a different pinout compared to J5A.
Yes, I have a datasheet of J5A, there is written about bootstrap mode , but without any circuit design.
Chip top marking is: MC68HC705J5ACP 1J48X ZRQQ0326
0 件の賞賛
返信

2,295件の閲覧回数
Alban
Senior Contributor II
The only pertinent info I found are:
 
AN499 Let the MC68HC705 Program Itself  -- pdf  -- 799 --  0 --  7/01/1996  
 
HC05J5AGRS 68HC(7)05J5A General Release Specification  -- pdf  -- 1419 --  2.1 --  3/14/2000
 
PA20SO1-08H-3(6) Programming Adapter  
(To be used with HC05 PRG I imagine)
 
M68HC05TB HC05 Family - Understanding Small Microcontrollers --  pdf --  2697 --   2  -- 1/01/1998
(Page 154: advise to use ICS)
 
Please note that this product is discontinued/obsolete : PCN10573
 
Alban.
 
0 件の賞賛
返信

2,295件の閲覧回数
Andik
Contributor II
Dear Alban,

These docs will not be useful, I'm affraid. There isn't the needed info. Anyhow, thank you for your effort. I appreciate it.
0 件の賞賛
返信