MC68705R3 erase

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC68705R3 erase

1,322 次查看
kamilica
Contributor I
Hi I am looking for solution to erase MC68705R3 chip. I have some with window on and they are UV erasable, but majority of them are without.
标签 (1)
0 项奖励
回复
1 回复

678 次查看
peg
Senior Contributor IV

Hello and welcome to the fora, kamilica.

Presumably the windowed ones are also ceramic with a quartz glass window. This is expensive to manufacture (buy) especially when most devices will only ever be programmed once. Because of this they come up with "OTP" One Time Programmable devices which are the same inside but just molded in plastic. If you need to re-programme these, you throw it away and use a new one.

This is probably what you have. If you don't want what is programmed into them now they are worthless.

 

0 项奖励
回复