MC1468705G2 information

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC1468705G2 information

4,554件の閲覧回数
Nihilist
Contributor I
Hello,

anyone got information about how to program / read / verify this old device ?
New programmers don't support it, and the old hardware which existed 20 years
ago is long lost.

Any help or ideas ?

Mike

ラベル(1)
0 件の賞賛
返信
7 返答(返信)

3,343件の閲覧回数
pierreriley
Contributor I

Hi All,

Was there any success to this? 

I would also like to know how to read this chip, like what hardware do I need. All help is much appreciated

Kind Regards

Pierre Riley. 

0 件の賞賛
返信

3,343件の閲覧回数
celsoken
Contributor V

Dear Pierre,

Pls google mc1468705g2, There is a PDF on Benoit page which is an old Moto AN. It programs itself. 

Cheers,

Celso

0 件の賞賛
返信

3,343件の閲覧回数
celsoken
Contributor V

And for reading you could check Reading the Eprom data from a vintage UV Eprom CPU Thanks to Matthieu Benoit for that!

Cheers,

Celso

0 件の賞賛
返信

3,343件の閲覧回数
peg
Senior Contributor IV
Hi Mike,

Try removing the 7 from your part number in a Google search.
This is not what you want but provides many hits that may lead you somewhere.

0 件の賞賛
返信

3,343件の閲覧回数
Nihilist
Contributor I
Hello,

thanks for your reply. The "7" means that it is an EPROM version of the controller,
so its needed :smileyhappy: I have found lots of information, but no real information about how
to program or read this controller. Somewhere was an old application note AN852
mentioned, but I didn't find it. Also, the AN1009 and AN1011 would be helpful, but
I can't find them on the net.

Its hard to find information for old devices...

Mike

0 件の賞賛
返信

3,343件の閲覧回数
celsoken
Contributor V
I feel like a dinossaurus from stone age, but I remember these parts.
I think they were one of the first of the 6805 CMOS generation.

Normally these parts programmed themselves, they had a boot rom wich was activated by high voltage (9V) in a pin, some used a CD4040 to generate address,  all controlled by the 6805.
Of course, you had to provide high voltage externally.

Unfortunately I put the old moto stuff in garbage can recently.
But if I could find one of these old stuff, I'll send it to you.

Cheers,

Celso
0 件の賞賛
返信

3,343件の閲覧回数
Nihilist
Contributor I
Hello Celso,

I understand what you mean. Its really old stuff I am looking for. I
already know that those devices could be monitored somehow.

The "normal" G" ( 705G2S ) can be read easily and also programmed.
Reading is done by verification of the contents ( detect A0 and CE, force
reset, present data, as an endless loop, and takes long. I have programmed
such a G2S with an external EPROM and I could get out the contents
within one week - dont laugh, it really took so long.). The EPROM file
was identical to the verified dump.

The problem is, that the G2L1 type cant go into verifying mode by grounding
VPP and switching -12V to IRQ, like the G2S.

The G2L1 is similiar to some SC and ZC commercial types, which also
cant be read out. They also dont want to go into verify mode. The software
works correct....

Michael
0 件の賞賛
返信