MC13234, How to make a PWM output?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC13234, How to make a PWM output?

ソリューションへジャンプ
1,150件の閲覧回数
Braulio_Cespede
Contributor III

Hi everyone.

 

I'm currently working on a project with the MC13234 (Zigbee Wireless micro-controller). I have to Implement a PWM  component output, but to be Honest, I don't even know how to make one.

 

Can someone help me?

 

With a Example I can make it through.

 

Thanks for Advanced.

ラベル(1)
0 件の賞賛
返信
1 解決策
991件の閲覧回数
iansmusical
Contributor V

Hello Braulio,

You'd probably be best looking at the TPM section of the MC13234 reference manual, assuming you understand what PWM is etc. Then have a look on the Freescale website for the HCS08QRUG document that shows a working example of using the TPM to generate PWM signals. Keep in mind that there are differences between TPM modules (and other modules) between some S08 variants.

Hope this helps :-)

Thanks,

Ian

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
992件の閲覧回数
iansmusical
Contributor V

Hello Braulio,

You'd probably be best looking at the TPM section of the MC13234 reference manual, assuming you understand what PWM is etc. Then have a look on the Freescale website for the HCS08QRUG document that shows a working example of using the TPM to generate PWM signals. Keep in mind that there are differences between TPM modules (and other modules) between some S08 variants.

Hope this helps :-)

Thanks,

Ian

0 件の賞賛
返信
991件の閲覧回数
Braulio_Cespede
Contributor III

Thank you for answer, I'm already done it.

Anyway I want to learn more about it, so I will find those documents and study a little.

Thanks again.

0 件の賞賛
返信
991件の閲覧回数
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. 8-bit Microcontrollers ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community.

0 件の賞賛
返信