MC1322x USB dongle

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC1322x USB dongle

2,542件の閲覧回数
Nyarlathotep
Contributor I

Hello everybody,

 

I'm looking for some description of the MC1322x USB dongle pre installed sniffer firmware (or for the source code of it).

I'd like to communicate with the device through virtual COM and I need to know what are the commands available.

Does anybody know where to find such a documentation?

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

1,369件の閲覧回数
tomlogic
Contributor III

It works with WireShark to capture packets.

 

Install WireShark and the WireShark ZigBee Utility.  You launch the utility from a command-prompt, passing in the COM port of the USB Dongle and the ZigBee channel you want to sniff.

 

Then you go into Wireshark and paste "\\.\pipe\wireshark" into the Interface field of teh Capture Options dialog.  Wireshark will then start displaying and decoding captured packets.

0 件の賞賛
返信