MC13224 Buck Regulator Usage problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC13224 Buck Regulator Usage problem

Jump to solution
3,319 Views
Elisa
Contributor III

I want to use a buck regulator on my MC13224 board. I'am using a code with codebase 3.0.4 ( Temperature Sensor) but it doesn't work.

 

If I don't solder the recommended external inductor of 100 μH ± 20% inductance (part TDK #SLF6028T-101MR42) and the external capacitor is a 10μF ceramic component, and solder the necessary 0 Ohm resistor, (= I don't use buck regulator) the node works perfectly and joins the network

 

If I use inductor and capacitor I have to modify the software (I have a 24MHz crystal).I did but it doesn't works.

 

I made this function:

 

void PowerUpBuck(void)
{
  
  crmVRegCntl_t VRegCntl;


  CRM_SetPowerSource(gCrmPwSBuckRegulation_c);


  /*buck*/
  VRegCntl.vReg = gBuckVReg_c;
  VRegCntl.BUCK_EN  = 1;//enable buck regulator
  VRegCntl.BUCK_SYNC_REC_EN = 1;//enable sync rectifier
  VRegCntl.BUCK_BYPASS_EN = 0 ;//Bypass disabled (default)
  VRegCntl.BUCK_CLK_DIV = gBuckClkDiv_15_c;

  CRM_VRegCntl(&VRegCntl);
  while(!CRM_VRegIsReady(V_REG_MASK_BUCK)){};


   /*NVM reg*/
  VRegCntl.vReg = g1P8VReg_c;
  VRegCntl.cntl.vReg1P8VEn =1;
  CRM_VRegCntl(&VRegCntl);
  while(!CRM_VRegIsReady(V_REG_MASK_1P8V)){};

 
  /*Analog reg*/
  VRegCntl.vReg = g1P5VReg_c;
  VRegCntl.VREG_1P5V_EN =gRxTxandPLLRegEnable_c;
  VRegCntl.VREG_1P5V_I_SEL =gARegCurent40mA_c;
  CRM_VRegCntl(&VRegCntl);
  while(!CRM_VRegIsReady(V_REG_MASK_1P5V)){}; 
 
//while (1) {};
  
}

 

I called it in BeeStackInit

 

void BeeStackInit(void) {
#if (gLpmIncluded_d || gComboDeviceCapability_d)
#if gComboDeviceCapability_d
  if(gLpmIncluded)
#endif
  {
    PWR_CheckForAndEnterNewPowerState_Init();
    PWRLib_SetCurrentZigbeeStackPowerState(StackPS_DeepSleep);
  }
#endif
  PowerUpBuck(); //added E.S. 16/07/2009

......

 

 If I stop the program using the while preceded by // at the end of PowerUpBuck functionand I use an oscilloscope I can se the quare ware on COIL_BK pin of MC13224 at 1.6MHz and I can see 2V on the capacitor. So it is working.

 

The problem is that if I don't stop the program, the node try to find the network.

 

Thi is what I can see with Test Tool:

 

Rx [17:42:29.718] MacScan.Confirm 84 0B 07 EA 01 00 00 00 00 00
    Header                         [2 bytes] = 84 0B
    PayloadLength                  [1 byte ] = 07
    Status                         [1 byte ] = EA (NO_BEACON)
    ScanType                       [1 byte ] = 01 (Active Scan)
    ResultListSize                 [1 byte ] = 00
    UnscannedChannels (only PS/AS) [4 bytes] = 00 00 00 00
    ResultList                     [0 bytes] = 

Rx [17:42:29.828] NLME-NETWORK-DISCOVERY.Confirm 97 41 02 00 EA
    Header            [2 bytes] = 97 41
    PayloadLength     [1 byte ] = 02
    NetworkCount      [1 byte ] = 00
    NetworkDescriptor [0 bytes] = 
    Status            [1 byte ] = EA (NO_BEACON)

Rx [17:42:29.921] NLME-NETWORK-DISCOVERY.Request 96 34 05 00 F8 FF 07 03
    Header        [2 bytes] = 96 34
    PayloadLength [1 byte ] = 05
    ScanChannels  [4 bytes] = 07 FF F8 00
    ScanDuration  [1 byte ] = 03

Rx [17:42:29.921] MacScan.Request 85 08 06 01 00 F8 FF 07 03
    Header        [2 bytes] = 85 08
    PayloadLength [1 byte ] = 06
    ScanType      [1 byte ] = 01 (Active Scan)
    ScanChannels  [4 bytes] = 07 FF F8 00
    ScanDuration  [1 byte ] = 03 

Labels (1)
0 Kudos
Reply
1 Solution
2,141 Views
Elisa
Contributor III

The problem at enabling the buck regulator was  corrected in BeeKit v1.9.9 release in August. The buck now works as indicated in the Reference Manual.

You can download the BeeKit v1.9.9, and the Software stack codebases will be upgraded within the BeeKit installation.

www.freescale.com/zigbee

View solution in original post

0 Kudos
Reply
2 Replies
2,141 Views
Elisa
Contributor III
Current codebases does not support buck regulator functionality, Currently Freescale is working to enable buck regulator on the upcoming releases, Very soon during next month August they will be available on Freescale webpage.
0 Kudos
Reply
2,142 Views
Elisa
Contributor III

The problem at enabling the buck regulator was  corrected in BeeKit v1.9.9 release in August. The buck now works as indicated in the Reference Manual.

You can download the BeeKit v1.9.9, and the Software stack codebases will be upgraded within the BeeKit installation.

www.freescale.com/zigbee

0 Kudos
Reply