MC13213 - modem issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC13213 - modem issue

2,405件の閲覧回数
Spell
Contributor I
I build a custom board using MC13213 for lighting application.
I use a relays for switch on and off the lamp.
Sometimes, after swtich on or off the lamp, the modem stops to work and restart after 4 minutes.
I suppose that problem is caused by an interference with the lamp switching circuit.
Can this delay depends on a software timeout? And is it programmable?
Can I check if the modem stops to work properly by some status registers or something else?
Thank you.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,525件の閲覧回数
Mads
Contributor V
Hi Spell,
 
if you are using your own written protocol, then please check our the Errata for the IC.
there is a subject about the timer3 that will set the Radio is idle mode and needs to be re-initiated into
receive mode again.
 
br,
Mads
0 件の賞賛
返信

1,525件の閲覧回数
Spell
Contributor I
Hi Mads,
I know about this issue but I'm using 802.15.4 MAC/PHY codebase so I think to be ok...

regards,
filippo
0 件の賞賛
返信