MC13213 RF Characterization Testing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC13213 RF Characterization Testing

1,776件の閲覧回数
GaryOlmstead
Senior Contributor I
Hi --
 
We are rolling our own ZigBee board with an MC13213.  For the required RF testing, we would like to be able to transmit continuously.  I don't see any way to do that.  Is there some undocumented test mode that would allow us to do this?
 
Gary Olmstead
Toucan Technology
Ventura CA
 
ラベル(1)
0 件の賞賛
返信
1 返信

1,004件の閲覧回数
Mads
Contributor V
Hi Gary,
 
My suggestion would be to used one of the documented ways :smileyhappy:
 
If you are using the SMAC you can use the Test mode application which contains all kinds of test features including continous TX.
 
if you are using Beestack or MACPHY you can use the "telec" test commands which are described in the MACPHY reference manual. these allows you to do Cont. Rx and TX.
 
Br,
Mads
0 件の賞賛
返信