[MC13213 - NCB] External antenna

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[MC13213 - NCB] External antenna

6,720 Views
CecchiSandrone
Contributor II
I want to increase the transmission range of the board 13213-NCB. I tried to attach a WLAN 2.4 GHz antenna to the plug but I can't see some benefits. May I must enable somewhere via software this type of antenna module or it isn't the right one?
Labels (1)
0 Kudos
Reply
9 Replies

2,991 Views
Spell
Contributor I
Hi Cecchi,
there is no module to enable via software. Are you sure that antenna have the right connector? is SMA or reverse SMA? Take a look to the connectors and check if there is the hot pole inside the plug.

regards,
Filippo
0 Kudos
Reply

2,991 Views
Spell
Contributor I
P.S.
Have you change the position of R111? If you take a look on schematic you can see for enable the external antenna you must move R111 in the R112 location.
0 Kudos
Reply

2,991 Views
CecchiSandrone
Contributor II

Attached you can see antenna and plug...there isn't an hot plug so the antenna is wrong. Where did you find schematics for 1321-NCB?

 

P1010017.jpg

P1010018.jpg

Message Edited by t.dowe on 2009-10-27 01:26 PM
0 Kudos
Reply

2,991 Views
Spell
Contributor I

You can use your WLAN antenna inserting manually a hot pole within the plug:smileywink:

I have attached the MC13213-NCB file.

 

1321xncb.zip

Message Edited by t.dowe on 2009-09-22 11:43 AM
0 Kudos
Reply

2,991 Views
CecchiSandrone
Contributor II
Unfortunately, I don't have a hot pole here...I must buy a "male" antenna. However, I don't understand this statement on the docs: "For RF measurements or for evaluating other antennas, connector J100 (SMA) can be enabled by moving a 0 Ohm jumper."
0 Kudos
Reply

2,991 Views
CecchiSandrone
Contributor II
So I must unweld R111 and move to the arrow position...
Obviously is it impossible to use both antennas together?



Message Edited by Cecchi Sandrone on 2007-11-27 10:25 AM

 

P1010020_copia.jpg

Message Edited by t.dowe on 2009-09-22 10:49 AM
0 Kudos
Reply

2,991 Views
Spell
Contributor I
Yes, it's impossible:smileywink:
0 Kudos
Reply

2,991 Views
Spell
Contributor I
For 0 ohm jumper is intended the 0 ohm resistor... you must move this resistor (R111) for enable the SMA connector.

You can made an hot pole using a piece of resistor terminal. I have made therefore:smileywink:
0 Kudos
Reply

2,991 Views
CecchiSandrone
Contributor II
Ah ok I found in my docs. However, It looks strange that to use an external antenna I must modify the board :smileymad:
Is it only a jumper? I don't understand where is...I don't see it on the board.


Message Edited by Cecchi Sandrone on 2007-11-27 09:47 AM
0 Kudos
Reply