MC13192 output impedance

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC13192 output impedance

3,819 次查看
xevi
Contributor I
Hi,
I'm designing a 802.15.4/ZigBee application and I can't find the output impedance off the transceiver MC13192. Seeing the design examples, I can deduce that it is 100 ohms, but am I right?
Also I'm interest in the S parameters off ZigBee antennas off development designs, can anybody help me?
 
Thx.
标签 (1)
0 项奖励
回复
2 回复数

933 次查看
J2MEJediMaster
Specialist I
Have you read the Freescale Application Note, "Compact Integrated Antennas Designs and Applications for the MC1319x, MC1320x, and MC1321x?" The note number is AN2731. It has a lot of information about interfacing antennae to this type of controller family. It says: "To interface with the MC1319x, the standard component 50–200 Ohm balun is recommended."

---Tom
0 项奖励
回复

933 次查看
AdamSch
Contributor I

In 1321x-ICB Development Board reference desing, component: 2450BL15B200 is used as balun. I dont see the point why is this exactly the right component for this interfacing cos its impedance is 200 Ohms on balanced side.

Unbalanced is 50 Ohms, which seems right to the antenna, but I dont understand why does it suppose to be 200 Ohms at modem side. I would appreciate if anyone can clear things up for me on this.

Thanks,

Adam 

0 项奖励
回复