Hello ramanoar,
For 10-bit accuracy, the equivalent source resistance at the ATD input pin should not exceed 10k ohm. This is the value of the parallel combination of the two resistors of the voltage divider. For example, if you chose resistor values of 10k (series) and 15k (shunt), this would give a source resistance of 6k ohm. A capacitor, typically 100nF, should also be connected between the input pin and ground.
However, this also assumes that your source resistance for the 5 volt signal is low. With the above voltage divider values, and for an error less than 1 LSB at 10-bit resolution, the source resistance should not exceed 240 ohms.
Regards,
Mac
Message Edited by bigmac on 2006-06-07 10:37 AM