M9S08QG8 doesn't run after some time in our application.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

M9S08QG8 doesn't run after some time in our application.

1,130 Views
roncanciovl
Contributor I
I have had problems using QG8, I program it by using CYCLONE programmer in production stage. I have programmed 5.000 chips for an automotive application. 20 of these have returned because they don't run. I check pins and they are in high impedance. However, if I reprogram the chips they work well again. I have not checked the memory because I protected it. I only read zeros.
 
Do you have any suggestions?
Labels (1)
0 Kudos
Reply
1 Reply

600 Views
bigmac
Specialist III
Hello,
 
On the failed units, do you test whether flash is blank or not?  Do you do a final test of each unit prior to shipping?
 
I think you need to rule out the possibility that the programming of a few devices might have been "missed".  It can easily happen.
 
Regards,
Mac
 
0 Kudos
Reply