M9KA2 marking code on a SOIC 8

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

M9KA2 marking code on a SOIC 8

3,568 次查看
admin
Specialist II

I have a circuit with a SOIC 8 IC marked with the code M9KA2. I think it is a Freescale microcontroller, but I'm not sure.

 

Could it be MC9RS08KA2?

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

2,259 次查看
admin
Specialist II

Hi,

Yes, I have a board designed a couple of years ago with that part and the component is marked M9KA2, next line is RMAKDC. Part is a MC9S08KA2 in SOIC8

Hope this helps,

--Rafa

0 项奖励
回复

2,259 次查看
lydia_ziegler
NXP Employee
NXP Employee

Hi,

It could be a new marking but the SOIC KA2's I have are marked with M9RS8KA2.  Do you see the little Freescale logo (looks like steps)?  There also should be 2 more lines of text.  The first is a letter code and the bottom is a date code.

Hope this helps!

0 项奖励
回复