M68EVB08GB60 software support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

M68EVB08GB60 software support

2,132 Views
anubhav
Contributor I
Dear all
 
i am working on M68EVB08GB60 demo board , i want to invoke the LCD through the POT attached at PTB0(ADC) port . please provide me the proper C code to run my application
Labels (1)
0 Kudos
Reply
1 Reply

1,139 Views
Jaux
Contributor I
I have developed an LCD interface for the AW60 chip, which is very similar to the GB60, only problem is the 3.3/5 V difference.

If you are after the code, I can let you have the s/w I have developed for the AW60.

It is written in Forth, and should be fairly easy to port to C/CodeWarrior

Let me know

J
0 Kudos
Reply