Looking for the cheapest 8 bit MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Looking for the cheapest 8 bit MCU

6,470 Views
tmyint
Contributor I
Hello,

What is the cheapest Freescale MCU I can find that has an A/D (8 bit is good enough) and a PWM generator? I have a fully licensed CodeWarrior for HC08 family so it would help me alot if the MCU is in this family. Thanks in advanced.

THM
Labels (1)
0 Kudos
Reply
6 Replies

3,017 Views
Z_C_Wang
NXP Employee
NXP Employee
MC9S08QD4:  8pin, $0.66, 4K/2K Flash,256/128 RAM, 8M Bus,4CH 10bits ADC, Two 16bit timers, 2.7V-5.5V,
The only thing is this device is a menmber of S08 family, not HC08. While, S08 has more advantages than HC08.
A low cost DEMO9S08QD4 board ($59.00) may be used during development.
Codewarrior Special Edition with free 16k-code-size-limite licence will work.
0 Kudos
Reply

3,017 Views
peg
Senior Contributor IV
Hi tmyint,
 
How about QT2A at $0.84/1000?
6-chan 10-bit AtoD, PWM 1536b FLASH
 
0 Kudos
Reply

3,017 Views
tmyint
Contributor I
thanks Peg and Weng, looks like this is what I will be using.
Peg sorry about the cross post.

Thet
0 Kudos
Reply

3,017 Views
tmyint
Contributor I
Hello,

What is the cheapest Freescale MCU I can find that has an A/D (8 bit is good enough) and a PWM generator? I have a fully licensed CodeWarrior for HC08 family so it would help me alot if the MCU is in this family. I can also do with just 8 pins. Thanks in advanced.

THM
0 Kudos
Reply

3,017 Views
peg
Senior Contributor IV
Hi again tmyint,
 
Please DO NOT cross post!
And this particular forum is definately the wrong place for this question!
Although you now know you got two independant answers for the same device.
 
0 Kudos
Reply

3,017 Views
rocco
Senior Contributor II
Hi, THM:

Have a look at the MC68HC908QT2. The QT2 has an 8 bit AtoD with a four channel analog multiplexer, and a timer module capable of both buffered and unbuffered PWM. The QT2 is in an 8-pin package, while it's larger sister, the QY2 is in a 16-pin package.

I don't know if it is the cheapest, but it is pretty darn cheap (under $1, last I heard).
0 Kudos
Reply