Looking for examples written in the book 'Zigbee Wireless Networking'

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Looking for examples written in the book 'Zigbee Wireless Networking'

2,122 Views
admin
Specialist II

Hello,

 

I'm a student at Technical University of Kosice/Slovakia and new in using Zigbee and Beekit. I try to follow this book (Zigbee Wireless Networking by Drew Gislason) to learn more about this enviroment. Like it is written in the book there should be examples at http://www.zigbookexamples.com/code. But there is only some for chapter 7 . It would be very nice if someone could help me to get all of these.

 

Thanks a lot

Matze

Labels (1)
0 Kudos
Reply
1 Reply

936 Views
Elisa
Contributor III

Hi Matze,

I had the same problem as you, so I wrote to Drew Giglason directly on June.

He replied me:

"Elisa,

I apologize, the full set of examples are not yet on the website. When they are, I'll ping you. Meanwhile, if you have any specific questions, I would be happy to answer them.
 
Regards,
Drew Gislason
San Juan Software
www.sanjuansw.com
"


But now there is nothing yet. Try to ask to the author...

 

Ciao,

Elisa

 

0 Kudos
Reply