Little documentation error in datasheet?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Little documentation error in datasheet?

1,379 Views
i_kauf
Contributor III

Hello All!

 

I was wondering about the Pin and connections diagram in MC9S08SE8 datasheet. The Timerchannel pins 26,25,22,21

should have the names TPM1CH0, TPM1CH1, TPM2CH0, TPM2CH1. Am I right? If so please tell me pin numbers for Timer channel two.

 

Regards,

 

Ingo   

Labels (1)
0 Kudos
Reply
1 Reply

1,127 Views
bigmac
Specialist III

Hello Ingo,

 

The 9S08SE8 device has two channels for TPM1, but only a single channel for TPM2.

 

The TPM1 channels will use pins 26 and 25, or alternatively pins 22 and 21, depending on the setting of the TPM1PS bit within the SOPT2 register.  TPM2CH0 uses pin 12.

 

Regards,

Mac

 

0 Kudos
Reply