LVI Queries

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LVI Queries

2,308 Views
Deepak1
Contributor IV

Dear All,
I am using MC68HC908JK8 devices My application VDD is 5v and I want to enable LVI at 2.49v.what modification I have to make in my code.
What are the possibilities If I have not enabled LVI.

Regards,

Deepak

Labels (1)
0 Kudos
Reply
2 Replies

1,506 Views
Lundin
Senior Contributor IV
It seems that the JK8 doesn't support 2.49V at 5V VDD. That makes sense since the minimum input voltage is specified to 0.7 * VDD.

0 Kudos
Reply

1,506 Views
Deepak1
Contributor IV
This means i have to set LVI Trip voltage at 4.25v for 5V operation ?
0 Kudos
Reply