LVI Queries

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LVI Queries

2,308件の閲覧回数
Deepak1
Contributor IV

Dear All,
I am using MC68HC908JK8 devices My application VDD is 5v and I want to enable LVI at 2.49v.what modification I have to make in my code.
What are the possibilities If I have not enabled LVI.

Regards,

Deepak

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,506件の閲覧回数
Lundin
Senior Contributor IV
It seems that the JK8 doesn't support 2.49V at 5V VDD. That makes sense since the minimum input voltage is specified to 0.7 * VDD.

0 件の賞賛
返信

1,506件の閲覧回数
Deepak1
Contributor IV
This means i have to set LVI Trip voltage at 4.25v for 5V operation ?
0 件の賞賛
返信