LCD drive problem - MC09S08LL16

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LCD drive problem - MC09S08LL16

2,277件の閲覧回数
Javercis
Contributor I
Hi everyone,
I have a LCD drive problem.

I want to drive a 8x24 LCD drive. LCD voltage is 3V and f = 51 Hz. via MC09S08LL16 microcontrller.

Problem;
When I set more than 3 segment on the same Frontplane the other segments are also appear but they are weak.

If I set only one segment this segment is also weak.
1 to 3 segment is working fine. The position of the segment doesnt care, but they must be on the same FP.

I hope someone can help me.





Message Edited by NLFSJ on 2009-02-02 06:24 AM
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,368件の閲覧回数
jag
Contributor IV
Try to put some external pullups on the lines. Bye Jack
0 件の賞賛
返信

1,368件の閲覧回数
Javercis
Contributor I
thanks for advise,

I change the configuration from Charge Pump enable to resistor devider enable and the problem is gone.

I hope the solution is not temporay..
Thanks ain for your attention...


0 件の賞賛
返信