LC60: TPM Input Capture Interrupt to wake up MCU in stop3 instead of KBI?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LC60: TPM Input Capture Interrupt to wake up MCU in stop3 instead of KBI?

1,510 Views
BasePointer
Contributor II
Hi,
 
Can I use Timer Input Capture Channel Interrupts to wake up MCU in stop3 mode, instead of KBI without consuming much power?
 
10x
BP.
Labels (1)
0 Kudos
Reply
1 Reply

612 Views
Ake
Contributor III
Hi,
 
In the MC9S08LC60 manual, rev 2, it says:
 
"Stop3 can be exited by asserting RESET, or by an interrupt from one of the following sources: the real-time interrupt (RTI), LVD, ADC, IRQ or the KBI."
 
The TPM is not included though, so it seems it won't work.
 
Regards,
Ake
0 Kudos
Reply