LC60: LVD resets MCU while the module is closed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LC60: LVD resets MCU while the module is closed

1,318 Views
BasePointer
Contributor II
Hi,
 
  // LVDF Low-Voltage Detect Flag
  // LVDACK Low-Voltage Detect Acknowledge
  // LVDIE Hardware interrupt disabled (use polling).
  // LVDRE Force an MCU reset when LVDF = 1.
  // LVDSE Low-voltage detect disabled during stop mode.
  // LVDE LVD logic disabled.
  // BGBE Bandgap Buffer disabled
  SPMSC1 = 0b01010000;
 
  // PDC Power down modes are disabled.
  SPMSC2 = 0b00000001;  // stop3
  
  // LVDV Low trip point selected (VLVD = VLVDL).
  // LVWV Low trip point selected (VLVW = VLVWL).
  SPMSC3 = 0b01000000;
 
The setting above causes MCU to reset with POR and LVD bit in SRS at mass production (ratio: 0.8%). I'm disabled bandgap buffer and LVD logic. I sometimes enable bandgap buffer to measure some external voltage and disable it immediately again. But never enable LVD logic.
 
Is that possible?
 
10x,
BP.
Labels (1)
0 Kudos
Reply
1 Reply

639 Views
BasePointer
Contributor II
Hi,
 
I wonder what is the mean of SRS register when it is equal to
0b10000000 -> only POR bit set
0b00000010 -> only LVD bits set
0b10000010 -> POR and LVD bits set *****
 
When I receive a reset with POR and LVD bits set in SRS, RAM content is still valid.
* The datasheet says that minimum RAM retention supply voltage is 1.0V.
* LVD threshold-low range is 1.76V-1.98V
* What is POR voltage (when does POR bit be set)?
* What is re-arm voltage indicated in the datasheet?
 
How can I take resets as POR and LVD bit set but with valid ram content?
 
Regards,
BP.


Message Edited by BasePointer on 2008-03-24 02:22 PM
0 Kudos
Reply