LC60: FLASH Characteristics

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LC60: FLASH Characteristics

1,623件の閲覧回数
BasePointer
Contributor II
Hi,
 
According to Table A-16. FLASH Characteristics in LC60 datasheet
 
Supply voltage for program/erase is 1.8 Vmin
 
Supply voltage for read operation
1.8 Vmin for 0 < fBus < 8 MHz and
2.08 V for 0 < fBus < 20 MHz
 
I also wonder the current consumption while erasing/programmin/reading the flash. The table doesn't indicate this.
 
Can I program the flash at 1.8V and -40C/+85C properly?
 
Thanks,
BP.
ラベル(1)
0 件の賞賛
返信
1 返信

1,023件の閲覧回数
Ake
Contributor III
Hello,
It seems like you have forgotten to ask the first question, so I will have to skip it.
Here are the answers to the following ones:
 
Yes, you can erase/program the Flash at all supply voltages.
 
The current consumption is not higher than the normal maximum values.
 
Yes you should be able to program the Flash EPROM at the minimum temperature without any problems.
 
Regards,
Ake
0 件の賞賛
返信