LC60: Debugging in Flash Emulation Routines

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LC60: Debugging in Flash Emulation Routines

2,720件の閲覧回数
BasePointer
Contributor II
Hi,
 
I'm storing some data in flash via flash emulation.
I can't see the written data in Memory window in True-Time Simulator after working flash emulation routines. Is this normal? Or it means my routines may have some problems?
 
I'm using CW6.0, HCS08 C and CyclonePro.
 
Thank you.
BP.


Message Edited by BasePointer on 2007-11-01 06:27 PM
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,524件の閲覧回数
Encoder
Contributor I
I find no problem to visualize Flash written blocks from running program on a MC9S08AW60 through BDM interface  and USB multilink or the USB interface on the MC9S08AWDEMO board and CW5.1.
Obviously you must stop the program to navigate in the memory, but you can resume when done. Flash routine, when physically writing or erasing flash cannot be halted (or at least I didn't try).
 
Encoder
0 件の賞賛
返信

1,524件の閲覧回数
BasePointer
Contributor II
Hi,
 
I think, it has some refresh problem.
 
Thanks.
0 件の賞賛
返信