L1934 : Fixup Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

L1934 : Fixup Error

3,551 次查看
CleverKnickname
Contributor I

Hello All,

 

I am currently migrating a project from the GB60 to the QE128 and I've come across the following linker errors:

 

Link Error   : L1934: ELF: Fixup error: Fixup error in '.debug_info' at offset 16ec

 

Link Error   : L1934: ELF: Fixup error: Fixup error in '.debug_frame' at offset 1b52

 

Link Error   : L1934: ELF: Fixup error: Fixup error in '.debug_pubnames' at offset 6

 

Link Error   : Link failed

 

This error was referenced by another thread here:

 

http://forums.freescale.com/freescale/board/message?board.id=16BITCOMM&message.id=6439

 

But no resolution was posted.

 

Any thoughts on this?  Has anyone else run into and resolved this issue?

 

Thanks

 

-JC

标签 (1)
0 项奖励
回复
2 回复数

1,647 次查看
CompilerGuru
NXP Employee
NXP Employee

Does the error persist when you delete the ..._Data folder?

Which versions of the tools are you using? How big is the project?

 

Did you file a service request?

Can you provide a reproducible case for the support (not for me :smileyhappy:.

 

Daniel

0 项奖励
回复

1,647 次查看
CleverKnickname
Contributor I

I have since resolved this issue by installing the compiler patch for CW 6.2.1. 

 

0 项奖励
回复