KIER 121 AND MC68HC908GP32

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KIER 121 AND MC68HC908GP32

1,651 Views
saxobross
Contributor I

I use codewarrior with the KIER121  and the kit microcontroller  MC68HC908GP32.
I use class 3 and mon 08 interface.
I made a simple programm to light the leds.
Then I have:
Attempting soft reset of HC08 device... Success. ( RSR=$48)
Initializing. Target has been RESET and is active.
CMD>CM C:\Program Files\Freescale\CodeWarrior for HC08 V5.1\prog\P&E\908_GP32.....
Initializing. (Bus Freq = 2466Khz) Initialized.
......
Loading programming algorithm.... Error writing data block to part. Disabling block write. Try again.
Error 14 during script !

If somebody could help me on that error 14, thanks
Labels (1)
0 Kudos
Reply
1 Reply

871 Views
peg
Senior Contributor IV
Hello and welcome to the fora, saxobross,

Perhaps no one has responded because they, like me, don't know what KIER121 is.
Maybe you could elaborate.

0 Kudos
Reply