JS16 Bootloader fails on USB3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

JS16 Bootloader fails on USB3

4,503 次查看
pgo
Senior Contributor V

Hi,

It appears that the JS16 ROM Bootloader fails on USB3 interfaces using the USBDM JS16Bootloader.

Has anyone else seen this other software.

Details about testing is available at:

JS16_Bootloader fails to program when using a USB 3 port · Issue #10 · podonoghue/usbdm-eclipse-make... 

thanks

标记 (2)
0 项奖励
回复
2 回复数

4,362 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

The S08JS family is old and the bootloader was released for USB 2.0 not for USB 3.0

Regards

0 项奖励
回复

4,362 次查看
pgo
Senior Contributor V

Hi Vincente,

I am aware the JS16 only supports USB2 BUT it should still work as a USB2 device on a USB3 interface since USB3 supports USB2 devices.  Otherwise we would have to throw away all our old devices which is not the case.

My USB2 software on the same device works fine on the same USB3 interface without any changes.

I would expect Freescale to be able to code to the USB2 specification and hence continue to work on current USB3 systems.

So I'm not sure what your reply is trying to indicate.

I am looking for confirmation that others have seen this problem so I know whether it is some subtle flaw in my bootloader GUI or a problem in the bootloader firmware.

bye

0 项奖励
回复