JM60 USB bootloader driver download

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JM60 USB bootloader driver download

5,650 Views
leesp
Contributor I

Hi,

Does anyone know where I can download the JM60 USB driver for Windows XP and Windows Embedded Standard 7?

Labels (1)
0 Kudos
Reply
5 Replies

3,450 Views
cesar_osorio
Contributor I

Hello, I have a problem with the JM60 USB bootloader driver. When I connect the EfmJM60 autoprogrammable module to a pc with windows XP, it works correctly, but when I work in a pc with windows 7, the pc detects the device with a name different to JM60 but the JMGui doesn't detect it. Should I install a special driver for windows 7? What must I do? I need your help. Thank you.

0 Kudos
Reply

3,450 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Augusto:

As SP Lee mentioned, you need a newer version of JM60 Bootloader GUI. Attached is what I think is the latest version available, and should be compatible with Windows 7.

:smileyalert: You have to uninstall previous versions of the GUI before running the installer.

Regards!

Jorge Gonzalez

0 Kudos
Reply

3,450 Views
leesp
Contributor I

Hi Cesar,

You need new driver for 64-bit. Below is the reply I got from FSL Technical Support:

"The installer version that I have sent you includes a
newer version of WinUSB driver, allowing compatibility with 64-bit Windows
versions. We have tested this version on Windows XP, Vista and Seven, on 32 and
64 bits and worked as expected, while the version available on the website is
compatible with 32-bit only. We are in process of upload the updated version on
the website.

   

Hope this will be useful for you. Please let me know if
you have further questions. Have a nice day.

Should you need to contact us with regard to this
message, please see the notes below.

Best Regards,

Carlos Jose

Technical Information & Commercial Support

Freescale Semiconductor"

0 Kudos
Reply

3,450 Views
J2MEJediMaster
Specialist I

The app note, AN3582 : The USB Data Logger based on the MC9S08JM60, describes a data logging application on a PC that uses the USB interface. The software for the app note is in the archive, AN3582SW.zip. This should help you get started.

 

---Tom

0 Kudos
Reply

3,450 Views
leesp
Contributor I

Dear J2MEJediMaster,

I mean the bootloader driver (Windows 7 - 64bit) for JM60.

I have JM60_GUI - which has the PC driver package including the WdfCoInstallerxxxxx.dll, WinUSBCoInstaller.dll and *.inf.

 

But I am not sure if these files can be used for Windows 7 64bit.

 

Please kindly advise. Thank you.

0 Kudos
Reply