JM60 Proyect design

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

JM60 Proyect design

跳至解决方案
2,258 次查看
hommmer
Contributor I

jmHi,

 

Im new to work with the JM60, and i have to make a proyect with it. I have been reading and i would like like to know if i'm right about the next process:

 

1. I have a MC9S08JM60CLD 44QFP

2. Then program the JM60 building a USBDM, like the one in the link:

http://usbdm.sourceforge.net/USBDM_V4.9/USBDM_JMxx/html/index.html

3. I need a special type of programming code using the USBDM?

4. When i have to programmed the JM60, how can i test if it works?, i have to desolder and place it (the JM60)  on a new  PCB for testing?

5. There is possible to made a cheap pcb to program and test?

 

Thanks

标签 (1)
标记 (4)
1 解答
2,064 次查看
eckhard
Contributor V

Hello,

you have to program the JM60 of the USBDM first with a BDM tool before you can use it. Only the JS16 version has a bootloader in ROM. So at first you have to get a BDM tool or build the JS16 version. The USBDM code and schematics can be found at sourceforges USBDM site. After Programming you can test the chip via the BDM tool.

You will go best if you build or get a JS16 USBDM for programming and debugging and test the JM60 in the circuit where it is needed.


Eckhard

在原帖中查看解决方案

3 回复数
2,064 次查看
Monica
Senior Contributor III

Hello Genner!

Was this suggestion helpful? Don't forget to keep us posted!

Best regards,

Monica

2,065 次查看
eckhard
Contributor V

Hello,

you have to program the JM60 of the USBDM first with a BDM tool before you can use it. Only the JS16 version has a bootloader in ROM. So at first you have to get a BDM tool or build the JS16 version. The USBDM code and schematics can be found at sourceforges USBDM site. After Programming you can test the chip via the BDM tool.

You will go best if you build or get a JS16 USBDM for programming and debugging and test the JM60 in the circuit where it is needed.


Eckhard

2,064 次查看
hommmer
Contributor I

Thanks very usefull info

0 项奖励
回复