JM60 Proyect design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JM60 Proyect design

Jump to solution
2,291 Views
hommmer
Contributor I

jmHi,

 

Im new to work with the JM60, and i have to make a proyect with it. I have been reading and i would like like to know if i'm right about the next process:

 

1. I have a MC9S08JM60CLD 44QFP

2. Then program the JM60 building a USBDM, like the one in the link:

http://usbdm.sourceforge.net/USBDM_V4.9/USBDM_JMxx/html/index.html

3. I need a special type of programming code using the USBDM?

4. When i have to programmed the JM60, how can i test if it works?, i have to desolder and place it (the JM60)  on a new  PCB for testing?

5. There is possible to made a cheap pcb to program and test?

 

Thanks

Labels (1)
1 Solution
2,097 Views
eckhard
Contributor V

Hello,

you have to program the JM60 of the USBDM first with a BDM tool before you can use it. Only the JS16 version has a bootloader in ROM. So at first you have to get a BDM tool or build the JS16 version. The USBDM code and schematics can be found at sourceforges USBDM site. After Programming you can test the chip via the BDM tool.

You will go best if you build or get a JS16 USBDM for programming and debugging and test the JM60 in the circuit where it is needed.


Eckhard

View solution in original post

3 Replies
2,097 Views
Monica
Senior Contributor III

Hello Genner!

Was this suggestion helpful? Don't forget to keep us posted!

Best regards,

Monica

2,098 Views
eckhard
Contributor V

Hello,

you have to program the JM60 of the USBDM first with a BDM tool before you can use it. Only the JS16 version has a bootloader in ROM. So at first you have to get a BDM tool or build the JS16 version. The USBDM code and schematics can be found at sourceforges USBDM site. After Programming you can test the chip via the BDM tool.

You will go best if you build or get a JS16 USBDM for programming and debugging and test the JM60 in the circuit where it is needed.


Eckhard

2,097 Views
hommmer
Contributor I

Thanks very usefull info

0 Kudos
Reply