JM60 @ 3.3V?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,869件の閲覧回数
ballen
Contributor I

I'm thinking of using the JM60 at 3.3V. The data sheet gives specs at 3V, so it must be ok, but I'm wondering why Vcc(typ) is listed at 5V. Are there any issues that aren't obvious? The only one that jumps out is the USB voltage regulator Vin(min) of 3.9V, which could easily be handled with a seperate supply.

 

Has anyone tried this? Anything unusual I should be aware of...?

Thanks,

bill

ラベル(1)
0 件の賞賛
返信
1 解決策
2,136件の閲覧回数
donw
Contributor IV

The JM60 works at full speed @ 3v3 OK. No catches except

for the USB supply as you note. (Disable the on board regulator and feed in

3v3 through a regulator from the USB Volt feed).

I connect port G0 (the next pin along) to the USB power pin, so I get a keyboard interrupt

when the USB is plugged in.

Note also for USB operation you need an external xtal 1 to 4 mhz.

And don't forget to set the Low Volt Detector to the correct trip voltage!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,137件の閲覧回数
donw
Contributor IV

The JM60 works at full speed @ 3v3 OK. No catches except

for the USB supply as you note. (Disable the on board regulator and feed in

3v3 through a regulator from the USB Volt feed).

I connect port G0 (the next pin along) to the USB power pin, so I get a keyboard interrupt

when the USB is plugged in.

Note also for USB operation you need an external xtal 1 to 4 mhz.

And don't forget to set the Low Volt Detector to the correct trip voltage!

0 件の賞賛
返信
2,136件の閲覧回数
ballen
Contributor I

Thanks, Don! Good idea on the KBI, too.

Bill

0 件の賞賛
返信