JBxx and USB ICP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

JBxx and USB ICP

4,576 次查看
peg
Senior Contributor IV
Hello,
 
The links to AN2398SW appear to be broken on this site. :smileysad:
Can it be fixed? Can I get it elsewhere?
 
Also apart from the brief mention in AN2399, is the blank part ICP mode of the JB16 documented somewhere? The JB16 manual only seems to be aware of serial mode. I find it a little difficult to believe that 1/2 Meg pulldowns on a USB would be noticed.
 
TIA
Peg
标签 (1)
0 项奖励
回复
3 回复数

1,363 次查看
Alban
Senior Contributor II
Hey Peg,
 
I think it's not documented because wasn't really for everyone at the start.
Maybe a big customer asked or someon suggested and it became the standard !
 
If we had heard before, Daniel would have made the TBDML (Turbo BDM Light, cheap programmer for S12) programmed from USB and the PCB would have been even smaller...
 
Ah "communication"...
 
Thanks for pinpointing the broken link.
 
Cheers,
Alban.
0 项奖励
回复

1,363 次查看
rocco
Senior Contributor II
Hi, Peg:

In case you can't find it anywhere else, I put a copy here:

http://www.remotehead.com/PrivateFolders/AN2398SWsoftware.zip

I also have the AN2399 software, if you need that as well.

Sorry I can't help on the ICP, except to agree that 1/2 mOhm pull-downs are not very significant.
0 项奖励
回复

1,363 次查看
Fonsi
Contributor I
If you have not gotten a hold of AN2398SW please submit an SR and as to be assigned to R23757.
 
Best Regards,
0 项奖励
回复