Hello;
If you are learning assembly a good start point could be the S08PT device; S08PT|8-bit 5V Full-featured MCU with EEPROM and TSI | NXP Semiconductors.
The software tool to use it is CodeWarrior for MCUs (Eclipse IDE) v11.1 available for windows 10/11.; in this tool you can test with assembly code as it have the tools view for debug in assembly and review the memory to understand the functionality of your code.
This device have an evaluation board S08PT60-EVK, [MC9S08PT60] if you are interested, [S08PT60-EVK Product Information] with various peripherals, for you to test different configurations from your code onto real hardware.
The onboard interfaces include an RGB LED, a 6-axis digital accelerometer and magnetometer, an ambient temperature sensor, two capacitive touch pads, a potentiometer, two user push-buttons, and IRDA transceiver. Also is compatible with the Arduino pin layout for expansions boards.
You can read more about the features in the main page: S08P MCUs Evaluation Kit | NXP Semiconductors
Best Regards, Luis